questions about mcf52211's USB module

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

questions about mcf52211's USB module

Jump to solution
3,177 Views
bluehacker
Contributor III

My question is if I must use 48MHZ crystal to use mcf52211's USB otg module?

thanks for your reply! 

Labels (1)
0 Kudos
Reply
1 Solution
2,028 Views
RichTestardi
Senior Contributor II

You don't have to use a 48MHz crystal.

 

The USB SIE, however, must run at 48MHz; the USB SIE can receive its clock from either the crystal oscillator, or from the PLL.

 

So...  If, for example, your crystal is 8MHz, then you can PLL its frequency up to 48MHz and run *both* the CPU and USB SIE from the PLL output.

 

The advantage of using a 48MHz crystal, however, is that you can run the CPU *faster* than 48MHz (say, 64MHz), and still have a 48MHz clock for the USB SIE (directly from the crystal oscillator).

 

Also see:

 

  http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&thread.id=5744

 

-- Rich

 

View solution in original post

0 Kudos
Reply
2 Replies
2,029 Views
RichTestardi
Senior Contributor II

You don't have to use a 48MHz crystal.

 

The USB SIE, however, must run at 48MHz; the USB SIE can receive its clock from either the crystal oscillator, or from the PLL.

 

So...  If, for example, your crystal is 8MHz, then you can PLL its frequency up to 48MHz and run *both* the CPU and USB SIE from the PLL output.

 

The advantage of using a 48MHz crystal, however, is that you can run the CPU *faster* than 48MHz (say, 64MHz), and still have a 48MHz clock for the USB SIE (directly from the crystal oscillator).

 

Also see:

 

  http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&thread.id=5744

 

-- Rich

 

0 Kudos
Reply
2,028 Views
bluehacker
Contributor III
thanks for your reply.
0 Kudos
Reply