questions about mcf52211's USB module

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

questions about mcf52211's USB module

跳至解决方案
3,213 次查看
bluehacker
Contributor III

My question is if I must use 48MHZ crystal to use mcf52211's USB otg module?

thanks for your reply! 

标签 (1)
0 项奖励
回复
1 解答
2,064 次查看
RichTestardi
Senior Contributor II

You don't have to use a 48MHz crystal.

 

The USB SIE, however, must run at 48MHz; the USB SIE can receive its clock from either the crystal oscillator, or from the PLL.

 

So...  If, for example, your crystal is 8MHz, then you can PLL its frequency up to 48MHz and run *both* the CPU and USB SIE from the PLL output.

 

The advantage of using a 48MHz crystal, however, is that you can run the CPU *faster* than 48MHz (say, 64MHz), and still have a 48MHz clock for the USB SIE (directly from the crystal oscillator).

 

Also see:

 

  http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&thread.id=5744

 

-- Rich

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,065 次查看
RichTestardi
Senior Contributor II

You don't have to use a 48MHz crystal.

 

The USB SIE, however, must run at 48MHz; the USB SIE can receive its clock from either the crystal oscillator, or from the PLL.

 

So...  If, for example, your crystal is 8MHz, then you can PLL its frequency up to 48MHz and run *both* the CPU and USB SIE from the PLL output.

 

The advantage of using a 48MHz crystal, however, is that you can run the CPU *faster* than 48MHz (say, 64MHz), and still have a 48MHz clock for the USB SIE (directly from the crystal oscillator).

 

Also see:

 

  http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&thread.id=5744

 

-- Rich

 

0 项奖励
回复
2,064 次查看
bluehacker
Contributor III
thanks for your reply.
0 项奖励
回复