questions about mcf52211's USB module

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

questions about mcf52211's USB module

ソリューションへジャンプ
3,216件の閲覧回数
bluehacker
Contributor III

My question is if I must use 48MHZ crystal to use mcf52211's USB otg module?

thanks for your reply! 

ラベル(1)
0 件の賞賛
返信
1 解決策
2,067件の閲覧回数
RichTestardi
Senior Contributor II

You don't have to use a 48MHz crystal.

 

The USB SIE, however, must run at 48MHz; the USB SIE can receive its clock from either the crystal oscillator, or from the PLL.

 

So...  If, for example, your crystal is 8MHz, then you can PLL its frequency up to 48MHz and run *both* the CPU and USB SIE from the PLL output.

 

The advantage of using a 48MHz crystal, however, is that you can run the CPU *faster* than 48MHz (say, 64MHz), and still have a 48MHz clock for the USB SIE (directly from the crystal oscillator).

 

Also see:

 

  http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&thread.id=5744

 

-- Rich

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,068件の閲覧回数
RichTestardi
Senior Contributor II

You don't have to use a 48MHz crystal.

 

The USB SIE, however, must run at 48MHz; the USB SIE can receive its clock from either the crystal oscillator, or from the PLL.

 

So...  If, for example, your crystal is 8MHz, then you can PLL its frequency up to 48MHz and run *both* the CPU and USB SIE from the PLL output.

 

The advantage of using a 48MHz crystal, however, is that you can run the CPU *faster* than 48MHz (say, 64MHz), and still have a 48MHz clock for the USB SIE (directly from the crystal oscillator).

 

Also see:

 

  http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&thread.id=5744

 

-- Rich

 

0 件の賞賛
返信
2,067件の閲覧回数
bluehacker
Contributor III
thanks for your reply.
0 件の賞賛
返信