problem in uclinux for Freescale™ V2 ColdFire Processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

problem in uclinux for Freescale™ V2 ColdFire Processor

3,055 Views
babaganoosh
Contributor I

 we have Freescale V2 ColdFire IP Core & SPP as IP.we are using xilinx as our fpga vendor.

we are trying to port uclinux 20080808 on our cold fire in fpga but some how it hang and if we give halt command from debugger we have communication error.(is it a known bug ???)
have any one of you have ever ported uclinux with this softcore,if yes then can you give us some examples, info or some source code as which linux is used and what are the procedures.

 

kind regards

Labels (1)
0 Kudos
Reply
4 Replies

2,033 Views
babaganoosh
Contributor I

have any one you guys worked with softcore 5208. iam trying to load linux kernal and having difficulties in it.

when we load linux kernal it goes andhangs at some place.may be some timer problem or some thing like this.

any suggestion , feedback .appreciated

 

regards

0 Kudos
Reply

2,034 Views
babaganoosh
Contributor I
i forget to mention about coldfire.iam having mcf5208.
0 Kudos
Reply

2,034 Views
JWW
Contributor V

babaganoosh,

 

Are you using the V2SPP from IPExtreme?

 

 

0 Kudos
Reply

2,034 Views
babaganoosh
Contributor I

yes iam using V2SPP from IPExtreme.

 

0 Kudos
Reply