problem in uclinux for Freescale™ V2 ColdFire Processor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

problem in uclinux for Freescale™ V2 ColdFire Processor

3,064件の閲覧回数
babaganoosh
Contributor I

 we have Freescale V2 ColdFire IP Core & SPP as IP.we are using xilinx as our fpga vendor.

we are trying to port uclinux 20080808 on our cold fire in fpga but some how it hang and if we give halt command from debugger we have communication error.(is it a known bug ???)
have any one of you have ever ported uclinux with this softcore,if yes then can you give us some examples, info or some source code as which linux is used and what are the procedures.

 

kind regards

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,042件の閲覧回数
babaganoosh
Contributor I

have any one you guys worked with softcore 5208. iam trying to load linux kernal and having difficulties in it.

when we load linux kernal it goes andhangs at some place.may be some timer problem or some thing like this.

any suggestion , feedback .appreciated

 

regards

0 件の賞賛
返信

2,043件の閲覧回数
babaganoosh
Contributor I
i forget to mention about coldfire.iam having mcf5208.
0 件の賞賛
返信

2,043件の閲覧回数
JWW
Contributor V

babaganoosh,

 

Are you using the V2SPP from IPExtreme?

 

 

0 件の賞賛
返信

2,043件の閲覧回数
babaganoosh
Contributor I

yes iam using V2SPP from IPExtreme.

 

0 件の賞賛
返信