mcf5253 external bus byte write

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

mcf5253 external bus byte write

跳至解决方案
1,918 次查看
Dec
Contributor III

Hi,

 

I'm looking at using the MCF5253 with a word wide SRAM on the external bus.

However, I cannot see any way of controlling which bytes of the data bus are active on a write.

Other MCF52XX chips I've used have a uppler/lower data bus strobe but this doesn't appear to have those.

 

Anybody done this before or knows what I'm missing ?

 

I see there have been similar questions to this for the mcf5249 on here but they didn't seem to get a reply/solution.

 

Thanks

标签 (1)
0 项奖励
回复
1 解答
1,402 次查看
Dec
Contributor III

The answer, via support, is that the writing of bytes to a word wide sram is not supported :smileysad:

 

Need to think of a plan-b quickly, sadly doesn't look like it's going to be Freescale :smileysad:

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,403 次查看
Dec
Contributor III

The answer, via support, is that the writing of bytes to a word wide sram is not supported :smileysad:

 

Need to think of a plan-b quickly, sadly doesn't look like it's going to be Freescale :smileysad:

0 项奖励
回复