mcf5253 external bus byte write

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mcf5253 external bus byte write

ソリューションへジャンプ
1,912件の閲覧回数
Dec
Contributor III

Hi,

 

I'm looking at using the MCF5253 with a word wide SRAM on the external bus.

However, I cannot see any way of controlling which bytes of the data bus are active on a write.

Other MCF52XX chips I've used have a uppler/lower data bus strobe but this doesn't appear to have those.

 

Anybody done this before or knows what I'm missing ?

 

I see there have been similar questions to this for the mcf5249 on here but they didn't seem to get a reply/solution.

 

Thanks

ラベル(1)
0 件の賞賛
返信
1 解決策
1,396件の閲覧回数
Dec
Contributor III

The answer, via support, is that the writing of bytes to a word wide sram is not supported :smileysad:

 

Need to think of a plan-b quickly, sadly doesn't look like it's going to be Freescale :smileysad:

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,397件の閲覧回数
Dec
Contributor III

The answer, via support, is that the writing of bytes to a word wide sram is not supported :smileysad:

 

Need to think of a plan-b quickly, sadly doesn't look like it's going to be Freescale :smileysad:

0 件の賞賛
返信