mcf5253 external bus byte write

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mcf5253 external bus byte write

Jump to solution
1,819 Views
Dec
Contributor III

Hi,

 

I'm looking at using the MCF5253 with a word wide SRAM on the external bus.

However, I cannot see any way of controlling which bytes of the data bus are active on a write.

Other MCF52XX chips I've used have a uppler/lower data bus strobe but this doesn't appear to have those.

 

Anybody done this before or knows what I'm missing ?

 

I see there have been similar questions to this for the mcf5249 on here but they didn't seem to get a reply/solution.

 

Thanks

Labels (1)
0 Kudos
Reply
1 Solution
1,303 Views
Dec
Contributor III

The answer, via support, is that the writing of bytes to a word wide sram is not supported :smileysad:

 

Need to think of a plan-b quickly, sadly doesn't look like it's going to be Freescale :smileysad:

View solution in original post

0 Kudos
Reply
1 Reply
1,304 Views
Dec
Contributor III

The answer, via support, is that the writing of bytes to a word wide sram is not supported :smileysad:

 

Need to think of a plan-b quickly, sadly doesn't look like it's going to be Freescale :smileysad:

0 Kudos
Reply