mcf52259 internal ram battery backup?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mcf52259 internal ram battery backup?

ソリューションへジャンプ
1,702件の閲覧回数
drummer
Contributor IV

I know that I read this somewhere but I can't find the reference for it.

A portion of the internal RAM is made non-volatile through the use of a battery connected to vstby.

I remember reading it somewhere. Does anyone know if it is the upper half or lower half that is retained?

Where is the reference for this information?

I am designing another product that may need to use this feature.

Thanks.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,625件の閲覧回数
TomE
Specialist II

Open the Reference Manual. Type "Control-F", search for "standby" and the first match will tell you.

Tom

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,626件の閲覧回数
TomE
Specialist II

Open the Reference Manual. Type "Control-F", search for "standby" and the first match will tell you.

Tom

0 件の賞賛
返信
1,625件の閲覧回数
drummer
Contributor IV

Thanks I knew I read it somewhere

• On-chip memories

— Up to 64-Kbyte dual-ported SRAM on CPU internal bus, supporting core, DMA, and USB

access with standby power supply support for the first 16 Kbytes

.

0 件の賞賛
返信