mcf52235

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mcf52235

1,713 Views
michaelkwan
Contributor I

I am currently designing a new circuit board with the MCF52235 device.  And, I ran out of board real estate to fit in a full 26-pin connector to support both debugging and programming/flashing the microcontroller.  What are the minimum signals/pins that I need to implement to support both debugging and programming/flashing functions. Are BDM port signal pin 1 to 10 out of the 26-pin connector all I needed? I can not find a sure/confident answer to support that from my researched resources/documents online.

Thanks!

Michael 

Labels (1)
0 Kudos
Reply
1 Reply

1,627 Views
miduo
NXP Employee
NXP Employee

Hi,

Please make reference from attached picture on the minimum BDM signals. Hope it is helpful.

0 Kudos
Reply