mcf52235

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mcf52235

1,837件の閲覧回数
michaelkwan
Contributor I

I am currently designing a new circuit board with the MCF52235 device.  And, I ran out of board real estate to fit in a full 26-pin connector to support both debugging and programming/flashing the microcontroller.  What are the minimum signals/pins that I need to implement to support both debugging and programming/flashing functions. Are BDM port signal pin 1 to 10 out of the 26-pin connector all I needed? I can not find a sure/confident answer to support that from my researched resources/documents online.

Thanks!

Michael 

ラベル(1)
0 件の賞賛
返信
1 返信

1,751件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

Please make reference from attached picture on the minimum BDM signals. Hope it is helpful.

0 件の賞賛
返信