linux startup problem on 548x (custom board)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

linux startup problem on 548x (custom board)

2,033 次查看
SridharS
Contributor I
Hi,
 
I have got linux-2.6.10 up & running on fire engine eval board (MCF5485) using the LTIB and BSP package provided by freescale . However when I run the same on a custom board , I get a trap at the point where it jumps to _running_high code after initializing the MMU in head.S . Any suggestions on where the problem could be ?
 
The only difference between the two setups is that in the latter , I use a BDM to single step and see where the problem is. I use colilo as the bootloader and I am able to the UART0 prints from colilo on my custom board, so I assume there is no problem there. The only change that I had to do in colilo is to change the RAM initilialization and change the clock frequency from 100mhz to 80mhz.
 
Also is there some tips/documentation available for changes needed to get linux up on a custom board running MCF54xx?
 
Thanks in advance,
Sridhar
标签 (1)
0 项奖励
回复
1 回复

1,210 次查看
JWW
Contributor V
Sridhar,

I'm not an expert on porting linux. But one common mistake is in the SDRAM init when moving from a Freescale board to a custom board. Sometimes it seems like the SDRAM is working, but when you enable cache and MMU you'll sometimes see problems arise. Try doing some DMA memory tests with a simple bootloader program or a codewarrior application to make sure your SDRAM init is robust.

-JWW
0 项奖励
回复