getting started with MCF52233

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

getting started with MCF52233

跳至解决方案
2,969 次查看
ridges
Contributor I

Hello,

My name is Martin. I'm interesting in develop an application with MCF52233.

The application work's over tcp/ip network. I have some MCF52233 demo board. I'ud like to use then as client and the PC as server. My question is if there are any aplication note about this. I have the AN 3518. But i dont know if trere are any others application notes or information.

The project consist in read an tri axis accelerometer in demo board (client) and transmit to the PC (sever) over TCP/IP network. This projet is for the university.

well thanks to all and i'll waiting for your answer...

Martin

标签 (1)
0 项奖励
回复
1 解答
2,213 次查看
MCF52233
Contributor III

Hi martin,

u can check out the coldfire lite project which includes many options like udp client , tcp client,

tcp serial client,http server.Also check application note AN3507:stck calculation ,AN3455:http server

,AN3470:tcp/ip stack and RTOS.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,214 次查看
MCF52233
Contributor III

Hi martin,

u can check out the coldfire lite project which includes many options like udp client , tcp client,

tcp serial client,http server.Also check application note AN3507:stck calculation ,AN3455:http server

,AN3470:tcp/ip stack and RTOS.

0 项奖励
回复
2,213 次查看
ridges
Contributor I

Hi,

 

Thank you very much for your recommendation. There is an example that is right for my application.

 

see you soon...

thanks again

Martin

0 项奖励
回复