getting started with MCF52233

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

getting started with MCF52233

ソリューションへジャンプ
2,985件の閲覧回数
ridges
Contributor I

Hello,

My name is Martin. I'm interesting in develop an application with MCF52233.

The application work's over tcp/ip network. I have some MCF52233 demo board. I'ud like to use then as client and the PC as server. My question is if there are any aplication note about this. I have the AN 3518. But i dont know if trere are any others application notes or information.

The project consist in read an tri axis accelerometer in demo board (client) and transmit to the PC (sever) over TCP/IP network. This projet is for the university.

well thanks to all and i'll waiting for your answer...

Martin

ラベル(1)
0 件の賞賛
返信
1 解決策
2,229件の閲覧回数
MCF52233
Contributor III

Hi martin,

u can check out the coldfire lite project which includes many options like udp client , tcp client,

tcp serial client,http server.Also check application note AN3507:stck calculation ,AN3455:http server

,AN3470:tcp/ip stack and RTOS.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,230件の閲覧回数
MCF52233
Contributor III

Hi martin,

u can check out the coldfire lite project which includes many options like udp client , tcp client,

tcp serial client,http server.Also check application note AN3507:stck calculation ,AN3455:http server

,AN3470:tcp/ip stack and RTOS.

0 件の賞賛
返信
2,229件の閲覧回数
ridges
Contributor I

Hi,

 

Thank you very much for your recommendation. There is an example that is right for my application.

 

see you soon...

thanks again

Martin

0 件の賞賛
返信