externam flash by MCF5329

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

externam flash by MCF5329

2,872 Views
Knopf
Contributor I
If i want programming in ciruet. the mfc5329 has to less memory. so i ndeed externel also. if i programming the MCF5329 over JTEC or other method does it use outomaticaly the external flash if the internal flash is full??
 
Or waht can i do or what shall i do?
 
Best thanks for help
 
Ralf
Labels (1)
0 Kudos
Reply
1 Reply

1,069 Views
UK_CF_FAE
NXP Employee
NXP Employee
Hi Ralf,
 
I'm pleased to hear that you are using the MCF5329. This device is a V3-core ColdFire part, with onchip USB and LCD controller.
 
MCF5329 has no internal flash memory, just on-chip RAM and cache. The evaluation board for the device is sold through Freescale but comes from LogicPD www.logicpd.com where you will find the schematics. These boards have 2MByte boot flash and some come with a further 16MB of flash. Normally, you'll run the application from external RAM.
 
The CFFlasher tool and Flash Programmer inside CodeWarrior have configuration files for the M5329EVB, so yes, they can program this external flash.
 
Mark
0 Kudos
Reply