Why the WP bit of flashbar register is always set?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why the WP bit of flashbar register is always set?

Jump to solution
801 Views
philippeloirat
Contributor I

Hi everybody,

We need to program flash memory of MCF52259 but the WP bit of flashbar register is always set??

Is somebody know why and how to change it?

Thanks to your reply.

Philippe

Labels (1)
0 Kudos
Reply
1 Solution
748 Views
TomE
Specialist II

It is always set to prevent you from writing to the address of the FLASH. That's clearly documented in section "18.3.2 Flash Base Address Register (FLASHBAR)".

Read section "1.5.4.2 Flash Memory", or the second "Note" in "18.3.2" to see how this works.

This came up in this Forum back in May, and searching for "backdoor" will get you two pages of hits going back to .

Re: Use of back door access

Prepare to be confused by the "backdoor flash address" versus the "backdoor key access".

Tom

View solution in original post

0 Kudos
Reply
1 Reply
749 Views
TomE
Specialist II

It is always set to prevent you from writing to the address of the FLASH. That's clearly documented in section "18.3.2 Flash Base Address Register (FLASHBAR)".

Read section "1.5.4.2 Flash Memory", or the second "Note" in "18.3.2" to see how this works.

This came up in this Forum back in May, and searching for "backdoor" will get you two pages of hits going back to .

Re: Use of back door access

Prepare to be confused by the "backdoor flash address" versus the "backdoor key access".

Tom

0 Kudos
Reply