Why the WP bit of flashbar register is always set?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why the WP bit of flashbar register is always set?

ソリューションへジャンプ
799件の閲覧回数
philippeloirat
Contributor I

Hi everybody,

We need to program flash memory of MCF52259 but the WP bit of flashbar register is always set??

Is somebody know why and how to change it?

Thanks to your reply.

Philippe

ラベル(1)
0 件の賞賛
返信
1 解決策
746件の閲覧回数
TomE
Specialist II

It is always set to prevent you from writing to the address of the FLASH. That's clearly documented in section "18.3.2 Flash Base Address Register (FLASHBAR)".

Read section "1.5.4.2 Flash Memory", or the second "Note" in "18.3.2" to see how this works.

This came up in this Forum back in May, and searching for "backdoor" will get you two pages of hits going back to .

Re: Use of back door access

Prepare to be confused by the "backdoor flash address" versus the "backdoor key access".

Tom

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
747件の閲覧回数
TomE
Specialist II

It is always set to prevent you from writing to the address of the FLASH. That's clearly documented in section "18.3.2 Flash Base Address Register (FLASHBAR)".

Read section "1.5.4.2 Flash Memory", or the second "Note" in "18.3.2" to see how this works.

This came up in this Forum back in May, and searching for "backdoor" will get you two pages of hits going back to .

Re: Use of back door access

Prepare to be confused by the "backdoor flash address" versus the "backdoor key access".

Tom

0 件の賞賛
返信