Where can I find dBug source code?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where can I find dBug source code?

2,677 Views
ljalvs
Contributor I

I can read in many posts that dBug sources are available to download from nxp website, but I can't find it...

The only thing I found was pre-compiled dBug's for a couple of evaluation boards.

Also, I'm not sure if it's bundled as a single package or one package per cpu type, but I'm looking dBug sources for mcf5206e, mcf5307 and mcf5407.

Can anyone help me? If the sources are no longer available, can someone share them?

THANKS!

Tags (1)
0 Kudos
Reply
3 Replies

2,565 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

I couldn't find MCF5307 and MCF5407 dBUG source code.

I attached MCF5206e dBUG source code for your reference.

Wish it helps.


Have a great day,
Mike

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,532 Views
Hacke3
Contributor I

Hi

How about source code for dBUG for MCF5206? I have an Arnewsh SBC5206 and interested in it's dBUG source.

Thanks,

Keith

0 Kudos
Reply

2,565 Views
ljalvs
Contributor I

Thanks a lot Hui_Ma!

Does anyone else have the sources for the other 2 cpu's? (mcf5407 and mcf5307).

0 Kudos
Reply