When is CCR.V bit set?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

When is CCR.V bit set?

ソリューションへジャンプ
3,308件の閲覧回数
tupdegrove
Contributor III

General question not related to specific device.  I understand it is an arithmetic overflow in simplest terms.  Wondering the specific instances where it is set. Tried to research on net and found two answers.

 

1.  XOR of a carry into the sign bit and a carry out of the sign bit.

 

2. For addition, set when positive num + positive num = positive num and when negative num + negative num = positive num.

 

For subtraction, set when negative num - positive num = negative num and when positive num - negative num = negative num.

 

Anyone have a good description?

 

Tim

ラベル(1)
0 件の賞賛
返信
1 解決策
2,324件の閲覧回数
kef
Specialist I

In real world, when we add positive number to positive number we expect positive answer. Sudden negative result is oVerflow.

 

Adding negative to negative shouold give negative result. Positive means oVerflow. 

 

And subtractiion is similar to addition, except the sign of one of addend.

 

HC12 CPU manual gives such V bit equation for ADD

V = D15 • M15 • /R15 + /D15 • /M15 • R15

 

where D15 sign bit of one addend, M15 - sign bit of second addend, R15 - sign bit of result.

So adding V is set when either 1) both arguments are positive and result negrative, or 2) when both args negative and result positive.

 

 

for SUB

V = D15 • /M15 • /R15 + /D15 • M15 • R15

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,325件の閲覧回数
kef
Specialist I

In real world, when we add positive number to positive number we expect positive answer. Sudden negative result is oVerflow.

 

Adding negative to negative shouold give negative result. Positive means oVerflow. 

 

And subtractiion is similar to addition, except the sign of one of addend.

 

HC12 CPU manual gives such V bit equation for ADD

V = D15 • M15 • /R15 + /D15 • /M15 • R15

 

where D15 sign bit of one addend, M15 - sign bit of second addend, R15 - sign bit of result.

So adding V is set when either 1) both arguments are positive and result negrative, or 2) when both args negative and result positive.

 

 

for SUB

V = D15 • /M15 • /R15 + /D15 • M15 • R15

0 件の賞賛
返信
2,324件の閲覧回数
tupdegrove
Contributor III

Thank-you for the details.

 

Just for the record, I meant to say:

 

2. For addition, set when positive num + positive num = negative num...

 

Tim

0 件の賞賛
返信