When is CCR.V bit set?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

When is CCR.V bit set?

Jump to solution
3,311 Views
tupdegrove
Contributor III

General question not related to specific device.  I understand it is an arithmetic overflow in simplest terms.  Wondering the specific instances where it is set. Tried to research on net and found two answers.

 

1.  XOR of a carry into the sign bit and a carry out of the sign bit.

 

2. For addition, set when positive num + positive num = positive num and when negative num + negative num = positive num.

 

For subtraction, set when negative num - positive num = negative num and when positive num - negative num = negative num.

 

Anyone have a good description?

 

Tim

Labels (1)
0 Kudos
Reply
1 Solution
2,327 Views
kef
Specialist I

In real world, when we add positive number to positive number we expect positive answer. Sudden negative result is oVerflow.

 

Adding negative to negative shouold give negative result. Positive means oVerflow. 

 

And subtractiion is similar to addition, except the sign of one of addend.

 

HC12 CPU manual gives such V bit equation for ADD

V = D15 • M15 • /R15 + /D15 • /M15 • R15

 

where D15 sign bit of one addend, M15 - sign bit of second addend, R15 - sign bit of result.

So adding V is set when either 1) both arguments are positive and result negrative, or 2) when both args negative and result positive.

 

 

for SUB

V = D15 • /M15 • /R15 + /D15 • M15 • R15

View solution in original post

0 Kudos
Reply
2 Replies
2,328 Views
kef
Specialist I

In real world, when we add positive number to positive number we expect positive answer. Sudden negative result is oVerflow.

 

Adding negative to negative shouold give negative result. Positive means oVerflow. 

 

And subtractiion is similar to addition, except the sign of one of addend.

 

HC12 CPU manual gives such V bit equation for ADD

V = D15 • M15 • /R15 + /D15 • /M15 • R15

 

where D15 sign bit of one addend, M15 - sign bit of second addend, R15 - sign bit of result.

So adding V is set when either 1) both arguments are positive and result negrative, or 2) when both args negative and result positive.

 

 

for SUB

V = D15 • /M15 • /R15 + /D15 • M15 • R15

0 Kudos
Reply
2,327 Views
tupdegrove
Contributor III

Thank-you for the details.

 

Just for the record, I meant to say:

 

2. For addition, set when positive num + positive num = negative num...

 

Tim

0 Kudos
Reply