USB TAP CCS Protocol Adapter error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB TAP CCS Protocol Adapter error

3,902件の閲覧回数
ZiglioNZ
Contributor I
CodeWarrior: 7.1
CPU: MCF54452

Hi everyone,

sometimes CodeWarrior fails to connect to the USB TAP in Debug Mode.
It seems to start normally but when I hit the break button, a pop up windows says:
"ColdFire CCS Protocol Adapter : Failed to stop the process"

That happens randomly, maybe once every 5 times. Has someone experienced the same nuisance and maybe found a solution?

I'm debugging off external RAM. The FREESCALE_USB-TAP settings are the following:

Connection Type: USB-TAP BDM
Use default Serial Number: enabled
CCS timeout: 10
Interface Clock Frequency: 5.120 MHz
Reset Target on Launch: Enabled

Thank you again,
Emanuel
ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,193件の閲覧回数
JWW
Contributor V
Did you ask this question in the Codewarrior forum yet?

-JWW

0 件の賞賛
返信

2,193件の閲覧回数
ZiglioNZ
Contributor I
Not yet, should I?
0 件の賞賛
返信

2,193件の閲覧回数
JWW
Contributor V
Yes.. The Codewarrior Moderators would be more knowledgeable  of the USB TAP.

I can move this thread... I think  :smileyhappy:
If you don't mind.

JWW
0 件の賞賛
返信

2,193件の閲覧回数
ZiglioNZ
Contributor I
That's fine for me, please do it

thanks,
Emanuel
0 件の賞賛
返信