USB TAP CCS Protocol Adapter error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB TAP CCS Protocol Adapter error

4,023 Views
ZiglioNZ
Contributor I
CodeWarrior: 7.1
CPU: MCF54452

Hi everyone,

sometimes CodeWarrior fails to connect to the USB TAP in Debug Mode.
It seems to start normally but when I hit the break button, a pop up windows says:
"ColdFire CCS Protocol Adapter : Failed to stop the process"

That happens randomly, maybe once every 5 times. Has someone experienced the same nuisance and maybe found a solution?

I'm debugging off external RAM. The FREESCALE_USB-TAP settings are the following:

Connection Type: USB-TAP BDM
Use default Serial Number: enabled
CCS timeout: 10
Interface Clock Frequency: 5.120 MHz
Reset Target on Launch: Enabled

Thank you again,
Emanuel
Labels (1)
0 Kudos
Reply
4 Replies

2,314 Views
JWW
Contributor V
Did you ask this question in the Codewarrior forum yet?

-JWW

0 Kudos
Reply

2,314 Views
ZiglioNZ
Contributor I
Not yet, should I?
0 Kudos
Reply

2,314 Views
JWW
Contributor V
Yes.. The Codewarrior Moderators would be more knowledgeable  of the USB TAP.

I can move this thread... I think  :smileyhappy:
If you don't mind.

JWW
0 Kudos
Reply

2,314 Views
ZiglioNZ
Contributor I
That's fine for me, please do it

thanks,
Emanuel
0 Kudos
Reply