We are using CMX USB-lite CDC driver on the ColdFire chip. With the BDM and Hiwave debugger running, the USB code works in wait mode. But without the BDM, the Host PC still enumerates our device but the COM port cannot be used. With BDM, our device draws 10mA more current which leads me to believe the MCU is still clocked. In fact, Ref. Manual says the MCU is clocked in stop modes if XCSR[BDMEN] bit is set.
We could not find anything that says definitely USB does or does not work in wait mode.
Hi z3,
We are facing very same problem. The reference manual said that USB is clocked in wait mode.
Anyone faced the same problem?
We are testing the code in the Freescale TWR-LCD kit. The source code is available in:
http://brtos.googlecode.com/files/TWR-LCD-FatFS.rar
This is a demo of BRTOS (real-time operating system) with eGUI, FAT32, SD card and CMX USB stack with CDC class (serial terminal).