UART interrupt on MCF5282EVB Lite

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UART interrupt on MCF5282EVB Lite

3,172件の閲覧回数
pch
Contributor I
I have been trying to get UART0 interrupt to work for the MCF5282EVB Lite.. the problem is that the isr is never called. I have noted and implemented all the suggestions in these forums and in the 5282UM, but I still cannot get this to work....
 
I have, however,  been able to get the PIT0 interrupt/isr to work on the 5282.
 
I also have a MCF5213EVB where I was able to successfully implement the UART interrupt and I tried to use the same method that worked in the 5213... but nothing seems to work on the 5282
 
What I need is a functional example/source for the 5282...
 
Does anyone have any UART/isr code that actually works?
 
Thanks... have a nice day.
ラベル(1)
0 件の賞賛
返信
1 返信

1,766件の閲覧回数
fire
Contributor I

hi,

 i did it long back.but now the cide is not with me.

if you send your code , i can find the bug and i can solve  it.

reply.

0 件の賞賛
返信