UART interrupt on MCF5282EVB Lite

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

UART interrupt on MCF5282EVB Lite

2,622 次查看
pch
Contributor I
I have been trying to get UART0 interrupt to work for the MCF5282EVB Lite.. the problem is that the isr is never called. I have noted and implemented all the suggestions in these forums and in the 5282UM, but I still cannot get this to work....
 
I have, however,  been able to get the PIT0 interrupt/isr to work on the 5282.
 
I also have a MCF5213EVB where I was able to successfully implement the UART interrupt and I tried to use the same method that worked in the 5213... but nothing seems to work on the 5282
 
What I need is a functional example/source for the 5282...
 
Does anyone have any UART/isr code that actually works?
 
Thanks... have a nice day.
标签 (1)
0 项奖励
回复
1 回复

1,216 次查看
fire
Contributor I

hi,

 i did it long back.but now the cide is not with me.

if you send your code , i can find the bug and i can solve  it.

reply.

0 项奖励
回复