TCP Client Abord-PowerOff Notification...

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TCP Client Abord-PowerOff Notification...

2,460 Views
SKumar
Contributor I
Hi all,
 
              I am using MCF52235 EVB on codewarrior environment.
              I am using uTaskser operating system.
 
              I have built up client server application.
              Problem is whenever client get shutdown in unusual way ( ie. Abort, Power off ) server not get
              notification that client is closed...which it get when we reset the board...
              
               Is anyone have any idea how to send notification to other board when any of two connected board get disconnected in unusual manner.
         
              Thank you.... 
 
 
Thanks,
kumar
Labels (1)
0 Kudos
Reply
2 Replies

1,483 Views
Nouchi
Senior Contributor II
Hi,

To detect which client is disconnected, server have to send periodically message to test client, if client does not respond in time, the server can consider the client disconnected.

Emmanuel
0 Kudos
Reply

1,483 Views
SKumar
Contributor I
Thanks a lot. That is great help.
 
kumar.
0 Kudos
Reply