Register reading for MCF 5282

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Register reading for MCF 5282

1,652件の閲覧回数
CHRamesh
Contributor I
hi,
 
Can anyone tell me, How to read the CPU space registers data(for e.g. VBR, FLASHBAR, RAMBAR, SR,....) of MCF5282.
I want to copy the register data to a variable.
I need the sample piece of code in C language for any one CPU Space registers
ラベル(1)
0 件の賞賛
返信
1 返信

1,015件の閲覧回数
RichTestardi
Senior Contributor II
I was under the impression CPU space was write-only.  The movec instruction says:
 
Description: Moves the contents of the general-purpose register to the specified control register. This transfer is always 32 bits even though the control register may be implemented with fewer bits. Note that the control registers are write only. The on-chip debug module can be used to read control registers. Note that this instruction synchronizes the pipeline.
 
You can remember every time you update a CPU space register (by shadowing the update to a static variable) and you can do that in C with a routine like this (which is resilient to whatever selected calling convention you are using):
 
static int
setvbr(uint32 x)
{
    asm {
        move  x,d0
        movec d0,vbr
    }
}
0 件の賞賛
返信