Re-compile gives different size

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Re-compile gives different size

1,935件の閲覧回数
tfd
Contributor I
I've the following "simple" problem: compiling the MSL_RuntimeCF.mcp project gives *.a files of different sizes (and contents) when compiled on two different machines. Obviously both PC have CodeWarrior 5.2.1174 and I've not changed anything in the project settings. Anybody has an idea why the libraries are different?

Thanks in advance,

Ronald
ラベル(1)
0 件の賞賛
返信
1 返信

1,051件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee
Do you look at the file size?
The elf files contain dates and most probably the cause for your differences, absolute paths (and maybe other things), so just checking the file size does not show much.
I would actually take the two *.a files, add them to a CW project, disassemble (context menu in the project) them and then compare the listing files.
0 件の賞賛
返信