QSPI Interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QSPI Interrupt

Jump to solution
3,286 Views
Stefan_75
Contributor II

Hi,

 

I am using the QSPI with enabled interrupt (SPIFE = 1) (ICM Sourcenb. 18). If I have to transfer some data, I put them in the queue and start the transfer. After that I continue with other C-programm parts.

When the finished interrupt (SPIF) occurs, I reset the interrupt flag in the SPI-intrrupt-routine and wait for the regular call of the SPI part and make my oprations.

 

The porgamm works well for some time, but after a few minutes the QSPI interrupt and all other normal interrupts won´t work any more (e.g. PIT).

 

Instead of the "normal" interrupts I get the interrupt nb. 58 which is "not used (reserved)" (Reference manual). 

 

Before I worked with the QSPI interrupt enable I made all the SPI traffic in one call (SPIFE = 0), and that worked fine. 

 

Does anybody knows what this interrupt (nb.58) mean, or has any suggestion? 

 

Target: MCF52235 

CW Version 7.1

Coldfire TCP Stack and RTOS

 

Thanks for any help.

 

Stefan

Labels (1)
0 Kudos
Reply
1 Solution
2,112 Views
admin
Specialist II

The reserved interrupt can happen due to overflow of interrupt stack or some buffer.

Check, if you disabled QSPI after the needed operations.

View solution in original post

0 Kudos
Reply
2 Replies
2,113 Views
admin
Specialist II

The reserved interrupt can happen due to overflow of interrupt stack or some buffer.

Check, if you disabled QSPI after the needed operations.

0 Kudos
Reply
2,112 Views
Stefan_75
Contributor II

Hi Yevgeni,

 

thanks for this answer. It seems to be an interrupt stack overflow. When the intrrupt occurs I disable the interrupt itself (SPIFE=0) and when I start a new transfer I enable it (SPIFE = 1). Now the system works well again.

 

Many thanks.

 

Stefan

0 Kudos
Reply