Power consumption of MCF54416CMJ250

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Power consumption of MCF54416CMJ250

1,741件の閲覧回数
sreejithrnair
Contributor I

@nxp 

Hi,

Could you kindly provide total power consumption of 

MCF54416CMJ250

0 件の賞賛
返信
3 返答(返信)

1,691件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please refer chapter 2.3 of MCF5441x datasheet about MCF5441x product power consumption.
For the total power consumption based on used modules, customer could use that specification to calculate the power consumption data.
For example: 
In run mode with nominal 1.2V the core power consumption is:
P=V(I)= 1.2(V) * 0.127(A)=0.15W

Wish it helps.

Mike

1,686件の閲覧回数
sreejithrnair
Contributor I

Thanks Hui.

 

0 件の賞賛
返信

1,722件の閲覧回数
TomE
Specialist II

That depends entirely on what you have it connected to, what modules inside it you're using, which power modes it is in for how long and how you've programmed it.

Have you read Section 2.3 (Power consumption specifications) in the Data Sheet?

Tom

 

0 件の賞賛
返信