Out of the box error [udp_send()] with project  ColdFire_Lite7x.mcp

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Out of the box error [udp_send()] with project  ColdFire_Lite7x.mcp

1,499 Views
Shotgun21
Contributor I

Hi everyone, this is my first post here. I just bought a ColdFire MCF52233DEMO. I downloaded the basic project: ColFire_Lite7x.mcp and when I run it on the board the red led COL lights up after about 30 seconds and I get the following error in the hyperterminal : Error sending via UDP tftp_udpsend(): udp_send() error -22.

 

I know the board works because when I took it out of the box it was connecting to my router and I could play with the examples from my internet browser. But now I can't put the project back in the board.

 

Can anyone help me please?

Labels (1)
0 Kudos
Reply
2 Replies

1,068 Views
Shotgun21
Contributor I

I have an update about my problem. Now the leds SPD LNK and ACT are on, but I can't connect to the webpage and here is the hyperterminal output:

 


Copyright 2006 by Freescale Semiconductor Inc.
Use of this software is controlled by the agreement
found in the project LICENSE.H file.
Built on Feb 21 2010 12:06:13

Heap size = 26112 bytes

IP Address = C0A80163
Gateway    = C0A80101
Mask       = FFFFFF00
etheraddr = 00:BA:smileyvery-happy:B:AD:01:02

Starting ints.
Calling netmain()...
InterNiche ColdFireLite TCP/IP for Coldfire, v3.0

Copyright 1997-2006 by InterNiche Technologies. All rights reserved.
Preparing device for networking
Ethernet started, Iface: 0, IP: 192.168.1.99
IP address of  : 192.168.1.99
INET> tftp_udpsend(): udp_send() error -22

Error sending via UDP

************************************************************

Is the board fried or is there a solution?

 

Thank you.

 

Math

0 Kudos
Reply

1,068 Views
mjbcswitzerland
Specialist V

Hi Math

 

Try another pre-built reference from here: http://www.utasker.com/SW_Demos.html

 

Download the SREC for your board with Codewarrior and see whether it runs (try pinging, FTP, TELNET, UART) as in following tutorial: http://www.utasker.com/docs/M5223X/uTaskerV1.3-Tutorial-M5223X_003.PDF

 

Regards

 

Mark

 

0 Kudos
Reply