Need 4 Uart Microcontroller in coldfire core-Please Help

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need 4 Uart Microcontroller in coldfire core-Please Help

2,394 Views
jai
Contributor I

Dears,

 

       I am new to Coldfire arch.I need Internal 4uart microcontroller(NOT processor) in Coldfire v1 or v2 family but I can't able to find.Please help

 

 Thanks in Advance

 

Thanks&Regards,

Jai

Labels (1)
0 Kudos
Reply
2 Replies

1,343 Views
gmnelson
Contributor III
As I am not aware of a V1 or V2 Coldfire that hasa total of 4 UARTS, why not go with the MCF52259 that that has 3 UARTS and then add an SPI UART such as the Maxim 3100 to the QSPI port which will provide you with a 4th UART.  I'm sure there are I2C UARTS that your could use as well.
0 Kudos
Reply

1,343 Views
MrBean
Contributor I

gmnelson wrote:
.....  I'm sure there are I2C UARTS that your could use as well.

eg. I2C uarts: Philips SC16IS7xx

0 Kudos
Reply