METHOD "POST" on mcf5223x

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

METHOD "POST" on mcf5223x

1,430 Views
FLATER
Contributor I
Hello... I want to use method post at embedded web server. Idon't know why is not supported. I try to change rcv buffer size but doesn't work for me. Can somebody help me?
Labels (1)
0 Kudos
Reply
1 Reply

877 Views
mjbcswitzerland
Specialist V

Hi

 

If you can't find a solution, take a look at the uTasker project. It supports posting files to the application or to the file system and also posting parameters. It operates with all browsers, as well as cURL. It also supports posting new (optionally encrypted) firmware to the target (boot loader).

 

This works on the M5223X and M5225X chips and can be completely tested in the uTaster simulator.

 

Regards

 

Mark

 

www.uTasker.com
- OS, TCP/IP stack, USB, device drivers and simulator for M5221X, M5222X, M5223X, M5225X. One package does them all - "Embedding it better..."

 

 

0 Kudos
Reply