MCU Programmer for MMC2114CFCAG33

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCU Programmer for MMC2114CFCAG33

5,106件の閲覧回数
CarmeltomC
Contributor II

We Used MMC2107CFCAG33 and CABLEMC M-Core Programmer, Due to the Obsolescence of above IC we have purchased MMC2114CFCAG33. Kindly tell me the Programmer Details, Compiler Details, and Programming Software required for compiling the OLD Code and Fusing the Object File into the IC. Kindly Support

Regards,

Carmel Tom,

[email protected]

タグ(1)
7 返答(返信)

5,029件の閲覧回数
TomE
Specialist II

The compiler should be the same as that for the old one. Have you lost the ability to compile the code for the old one? That's a problem.

Have you checked the document detailing the hardware and software differences between the two chips? Some of these may require you to make changes to the source code, then test those changes.

 https://www.nxp.com/docs/en/application-note/AN2286.pdf

Tom

 

4,958件の閲覧回数
CarmeltomC
Contributor II
0 件の賞賛
返信

5,042件の閲覧回数
TomE
Specialist II

The MMC2107CFCAG33 went EOL in 2019. The MMC2114CFCAG33 went EOL in 2020.

These products are usually only supported for development and programming when they're new. For these chips, that was at least 22 years ago, back in 2002 for the 2114 and 2000 for the 2107.

The best you could do is to have someone find an old one in a cupboard that's been there for 20 years. This is the Coldfire Forum, so isn't the "right one" for finding those people. Search all forums for "MMC2114" and follow the similar questions starting from 2009 in "Legacy Codewarrior" ("support has been discontinued") and "Other NXP Products" (links to Lauterbach and other ones).

Being in the same family, the programmer you're using for the 2107 should be a starting point for programming the 2114. The interface (whatever it is) should be similar. One problem I can see is that the 2114 uses "Second generation FLASH for M•CORE", which is different to the previous one. So the code that generates the programming sequences is probably different.

The Lauterbach link (following the link that NXP Support provided in 2022) looks promising:

https://www.lauterbach.com/supported-platforms/chips/mmc2114/Essential-Debugger-with-USB#wizard-step...

Tom

 

4,957件の閲覧回数
CarmeltomC
Contributor II
0 件の賞賛
返信

5,096件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

I could find below support record at P&E Micro website about MCore programmer.

https://www.pemicro.com/forums/forum_topic.cfm?forum_id=11&forum_topic_id=7632

It looks like P&E company discontinue to provide MCore related programmer tool.

Could you check with P&E support team if there with any updated info about MCore programmer tool.

Sorry for that.

Mike

4,956件の閲覧回数
CarmeltomC
Contributor II
0 件の賞賛
返信

5,046件の閲覧回数
CarmeltomC
Contributor II

Noted Thanks...We have purchased this IC for our production use, We have to use it now, and what is the way or solution? how can i program? kindly support...

0 件の賞賛
返信