MCF548x CLKIN to PLL?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF548x CLKIN to PLL?

ソリューションへジャンプ
2,794件の閲覧回数
zwilcox
Contributor IV

I'm trying to hook up a crystal to the MCF5484.  

There's a CLKIN line where it looks like the crystal hooks up to.  Usually there's like a CLKOUT or osc_out, xtal_out or something but I'm not seeing that.

This is what I have so far:
pastedImage_1.png

Am I missing something?

Thanks in advance
Zach

Edit:  Here's the full module for the Test, Reset, and Clock portion
pastedImage_1.png

1 解決策
2,599件の閲覧回数
TomE
Specialist II

The Data Sheet has a section on the PLL detailing the CLKIN signal in "Table 7. Clock Timing Specifications". The levels and rise time can only be obeyed with an external hybrid oscillator, not a crystal.

In the Reference Manual:

10.1.2  Clocking Overview
The MCF548x requires a clock generated externally to be input to the CLKIN signal.

Tom

元の投稿で解決策を見る

6 返答(返信)
2,599件の閲覧回数
miduo
NXP Employee
NXP Employee

Hello,

Actually the M5485EVB is not designed by NXP(Freescale). It was developed by LogicPD. However we had an internal evaluation board which was for internal test. The above schematic is from this board.

2,600件の閲覧回数
TomE
Specialist II

The Data Sheet has a section on the PLL detailing the CLKIN signal in "Table 7. Clock Timing Specifications". The levels and rise time can only be obeyed with an external hybrid oscillator, not a crystal.

In the Reference Manual:

10.1.2  Clocking Overview
The MCF548x requires a clock generated externally to be input to the CLKIN signal.

Tom

2,599件の閲覧回数
zwilcox
Contributor IV

Ahh ok.  Cool thanks.   I'll need to fix this.  That helps. 

0 件の賞賛
返信
2,599件の閲覧回数
TomE
Specialist II

I've just received email on this thread from you (Zachary) asking for the schematics for the ref board. As of this time the post isn't visible here, so I guess it'll get there before this one does.

Anyway...

On the NXP MCF5485 Page under the "Software and Tools" tab there are two "Reference Board" packages. These contain schematics.

Tom

2,599件の閲覧回数
miduo
NXP Employee
NXP Employee

Hello,

Please see our evaluation board for the clock scheme:

pastedImage_1.png

2,599件の閲覧回数
zwilcox
Contributor IV

Hey miduo‌!

Would you be able to provide the schematic for the eval board? 
I don't see it listed here MCF5485 Evaluation Board|NXP 

Thanks :smileyhappy:

0 件の賞賛
返信