MCF5485EVB : ltib kernel building problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF5485EVB : ltib kernel building problem

ソリューションへジャンプ
3,317件の閲覧回数
schiller
Contributor III

Hi all,

 

I'm using ltib20080808 for my MCF5485EVB board. Everyhting was running good until today. I'm currently working on the Linux kernel and I use quite often the ltib -c configuration mode to customize my kernel. I have been using this command for several months now without any problem. Today, while executing the ltib -c command, I got this error message :

 

 

 Processing: kernel-2.6.25-mcfv4e==================================Build path taken because: build key set, no prebuilt rpm,rpmbuild --dbpath /work/MCF5485EVB/ltib-m5475evb-20080808/rootfs//home/rpmdb --target m68k --define '_unpackaged_files_terminate_build 0' --define '_target_cpu m68k' --define '__strip strip' --define '_topdir /work/MCF5485EVB/ltib-m5475evb-20080808/rpm' --define '_prefix /usr' --define '_tmppath /work/MCF5485EVB/ltib-m5475evb-20080808/tmp' --define '_mandir /usr/share/man' --define '_sysconfdir /etc' --define '_localstatedir /var' -bb --clean --rmsource  /work/MCF5485EVB/ltib-m5475evb-20080808/rpm/SPECS/kernel-2.6.25-mcfv4e.specBuilding target platforms: m68kBuilding for target m68kExecuting(%prep): /bin/sh -e /work/MCF5485EVB/ltib-m5475evb-20080808/tmp/rpm-tmp.62856+ umask 022+ cd /work/MCF5485EVB/ltib-m5475evb-20080808/rpm/BUILD+ exit 0Executing(%build): /bin/sh -e /work/MCF5485EVB/ltib-m5475evb-20080808/tmp/rpm-tmp.62856+ umask 022+ cd /work/MCF5485EVB/ltib-m5475evb-20080808/rpm/BUILD+ exit 0Executing(%install): /bin/sh -e /work/MCF5485EVB/ltib-m5475evb-20080808/tmp/rpm-tmp.62856+ umask 022+ cd /work/MCF5485EVB/ltib-m5475evb-20080808/rpm/BUILDProcessing files: kernel-2.6.25-1error: File not found by glob: /work/MCF5485EVB/ltib-m5475evb-20080808/tmp/kernel/opt/freescale/rootfs/m68k/*RPM build errors:    File not found by glob: /work/MCF5485EVB/ltib-m5475evb-20080808/tmp/kernel/opt/freescale/rootfs/m68k/*Build time for kernel-2.6.25-mcfv4e: 0 secondsFailed building kernel-2.6.25-mcfv4ef_buildrpms() returned an error, exitingtraceback: main:501Started: Mon Aug 24 11:52:41 2009Ended:   Mon Aug 24 11:52:42 2009Elapsed: 1 secondsThese packages failed to build:kernel-2.6.25-mcfv4eBuild FailedExiting on error or interrupt

 

 

 

I'm really stuck trying to see where it could come from but to be honest I'm new to rpm and I'm totally lost. 

Is there somebody here who have already encountered this kind of problem ?

If yes, how can I solve that ?

 

Thanks for your help!

ラベル(1)
0 件の賞賛
返信
1 解決策
1,940件の閲覧回数
schiller
Contributor III

Ok guys, I get it. My file  /work/MCF5485EVB/ltib-m5475evb-20080808/rpm/SPECS/kernel-2.6.25-mcfv4e.spec was very strange (nothing in the %Build ans so on...). Just delete it and re-run ltib -c and everything goes well. No idea why this file has been corrupted...

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,941件の閲覧回数
schiller
Contributor III

Ok guys, I get it. My file  /work/MCF5485EVB/ltib-m5475evb-20080808/rpm/SPECS/kernel-2.6.25-mcfv4e.spec was very strange (nothing in the %Build ans so on...). Just delete it and re-run ltib -c and everything goes well. No idea why this file has been corrupted...

0 件の賞賛
返信
1,940件の閲覧回数
admin
Specialist II
I know this is very pld thread. Anyway this problem is related to me. I am not having this kernel spec file in that SPECS directory. That directory is empty
0 件の賞賛
返信