MCF5485EVB : ltib kernel building problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MCF5485EVB : ltib kernel building problem

跳至解决方案
2,354 次查看
schiller
Contributor III

Hi all,

 

I'm using ltib20080808 for my MCF5485EVB board. Everyhting was running good until today. I'm currently working on the Linux kernel and I use quite often the ltib -c configuration mode to customize my kernel. I have been using this command for several months now without any problem. Today, while executing the ltib -c command, I got this error message :

 

 

 Processing: kernel-2.6.25-mcfv4e==================================Build path taken because: build key set, no prebuilt rpm,rpmbuild --dbpath /work/MCF5485EVB/ltib-m5475evb-20080808/rootfs//home/rpmdb --target m68k --define '_unpackaged_files_terminate_build 0' --define '_target_cpu m68k' --define '__strip strip' --define '_topdir /work/MCF5485EVB/ltib-m5475evb-20080808/rpm' --define '_prefix /usr' --define '_tmppath /work/MCF5485EVB/ltib-m5475evb-20080808/tmp' --define '_mandir /usr/share/man' --define '_sysconfdir /etc' --define '_localstatedir /var' -bb --clean --rmsource  /work/MCF5485EVB/ltib-m5475evb-20080808/rpm/SPECS/kernel-2.6.25-mcfv4e.specBuilding target platforms: m68kBuilding for target m68kExecuting(%prep): /bin/sh -e /work/MCF5485EVB/ltib-m5475evb-20080808/tmp/rpm-tmp.62856+ umask 022+ cd /work/MCF5485EVB/ltib-m5475evb-20080808/rpm/BUILD+ exit 0Executing(%build): /bin/sh -e /work/MCF5485EVB/ltib-m5475evb-20080808/tmp/rpm-tmp.62856+ umask 022+ cd /work/MCF5485EVB/ltib-m5475evb-20080808/rpm/BUILD+ exit 0Executing(%install): /bin/sh -e /work/MCF5485EVB/ltib-m5475evb-20080808/tmp/rpm-tmp.62856+ umask 022+ cd /work/MCF5485EVB/ltib-m5475evb-20080808/rpm/BUILDProcessing files: kernel-2.6.25-1error: File not found by glob: /work/MCF5485EVB/ltib-m5475evb-20080808/tmp/kernel/opt/freescale/rootfs/m68k/*RPM build errors:    File not found by glob: /work/MCF5485EVB/ltib-m5475evb-20080808/tmp/kernel/opt/freescale/rootfs/m68k/*Build time for kernel-2.6.25-mcfv4e: 0 secondsFailed building kernel-2.6.25-mcfv4ef_buildrpms() returned an error, exitingtraceback: main:501Started: Mon Aug 24 11:52:41 2009Ended:   Mon Aug 24 11:52:42 2009Elapsed: 1 secondsThese packages failed to build:kernel-2.6.25-mcfv4eBuild FailedExiting on error or interrupt

 

 

 

I'm really stuck trying to see where it could come from but to be honest I'm new to rpm and I'm totally lost. 

Is there somebody here who have already encountered this kind of problem ?

If yes, how can I solve that ?

 

Thanks for your help!

标签 (1)
0 项奖励
回复
1 解答
977 次查看
schiller
Contributor III

Ok guys, I get it. My file  /work/MCF5485EVB/ltib-m5475evb-20080808/rpm/SPECS/kernel-2.6.25-mcfv4e.spec was very strange (nothing in the %Build ans so on...). Just delete it and re-run ltib -c and everything goes well. No idea why this file has been corrupted...

在原帖中查看解决方案

0 项奖励
回复
2 回复数
978 次查看
schiller
Contributor III

Ok guys, I get it. My file  /work/MCF5485EVB/ltib-m5475evb-20080808/rpm/SPECS/kernel-2.6.25-mcfv4e.spec was very strange (nothing in the %Build ans so on...). Just delete it and re-run ltib -c and everything goes well. No idea why this file has been corrupted...

0 项奖励
回复
977 次查看
admin
Specialist II
I know this is very pld thread. Anyway this problem is related to me. I am not having this kernel spec file in that SPECS directory. That directory is empty
0 项奖励
回复