MCF5475CFE PCI Controller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF5475CFE PCI Controller

1,800件の閲覧回数
mniuser
Contributor I
For a breadboard we are designing, we are using 2 Fire Engine modules mounted on a host board. The final design will be using the PCI bus for communication between Coldfire processors. I would like to connect both Fire Engine MCF5475s to the same PCI bus on the host board, but have encountered two issues.   
1.  The PCI clock for the FE is supplied by the clock on board.   I don't see a way to provide an outside clock source, so cannot put both processors on the same PCI clock source.
2.  The PCI_IDSEL line is hardwired to PCI_AD16.   (This is used for Type 0 Configuration).  I think that this can be overcome by software though, which would be okay for breadboard purposes.
 
Any suggestions on how to get around the clock issue?
ラベル(1)
0 件の賞賛
返信
1 返信

1,357件の閲覧回数
kmahan
Contributor I
My comment isn't specifically related to you're question, but since you are using PCI on the fireengines please read the release note (the section on PCI) in the latest BSP.
0 件の賞賛
返信