MCF5271

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCF5271

2,931 次查看
diep
Contributor I

Hi all

I am studing MCF5271. I have some questions. I hope everybody help me.

1. I want to use uCLinux. What should I use software, tool and programmer to write code, debug and programmer for MCF5271?

2. What different are JTAG and BDM? I should JTAG or BDM to programmer for MCF5271.

Thank

标签 (1)
0 项奖励
回复
3 回复数

2,278 次查看
Replika
Contributor I

I am new to ColdFire and also looking for a cheap development environment for the chip (MCF5271) on Linux.

Does anybody suggest a solution (hardware/software/driver) to program the chip above, (debugging is optional)

Does bdm.sourceforce.net work with my chip? Which cable needed to flash it?

0 项奖励
回复

2,278 次查看
Replika
Contributor I

[pump]

 

I plan to use codesourcery toolchains (http://www.codesourcery.com/sgpp/lite/coldfire) to port uClinux on that chip.

Does anyone know (free) a flasher tool runs on Linux?

If I use CF FLasher on WIndows, is it compatible with this P&E device and the toolchains.

 

Thanks in advance.

 

0 项奖励
回复

2,278 次查看
bluehacker
Contributor III

there are bdm pod can use in linux, but I never try it. currently, I use BDM burn bootloader into flash under windows host with codewarrior. then use bootloader to download kernelimage.

 

freescale offers open source BDM for coldfire, and there are also another open source bdm named USBDM. if you are in china mainland, plaease see: http://nicrosystem.taobao.com

0 项奖励
回复