MCF5271

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF5271

2,929件の閲覧回数
diep
Contributor I

Hi all

I am studing MCF5271. I have some questions. I hope everybody help me.

1. I want to use uCLinux. What should I use software, tool and programmer to write code, debug and programmer for MCF5271?

2. What different are JTAG and BDM? I should JTAG or BDM to programmer for MCF5271.

Thank

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,276件の閲覧回数
Replika
Contributor I

I am new to ColdFire and also looking for a cheap development environment for the chip (MCF5271) on Linux.

Does anybody suggest a solution (hardware/software/driver) to program the chip above, (debugging is optional)

Does bdm.sourceforce.net work with my chip? Which cable needed to flash it?

0 件の賞賛
返信

2,276件の閲覧回数
Replika
Contributor I

[pump]

 

I plan to use codesourcery toolchains (http://www.codesourcery.com/sgpp/lite/coldfire) to port uClinux on that chip.

Does anyone know (free) a flasher tool runs on Linux?

If I use CF FLasher on WIndows, is it compatible with this P&E device and the toolchains.

 

Thanks in advance.

 

0 件の賞賛
返信

2,276件の閲覧回数
bluehacker
Contributor III

there are bdm pod can use in linux, but I never try it. currently, I use BDM burn bootloader into flash under windows host with codewarrior. then use bootloader to download kernelimage.

 

freescale offers open source BDM for coldfire, and there are also another open source bdm named USBDM. if you are in china mainland, plaease see: http://nicrosystem.taobao.com

0 件の賞賛
返信