MCF52252 flash memory block

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF52252 flash memory block

ソリューションへジャンプ
2,403件の閲覧回数
LPs1978
Contributor III

Hi all,

    a simple question, only to be sure.

 

I'm going to use a MCF52252 and I read on manual that the flash memory is divided into 4Kbytes blocks.

 

Is this true? My doubt is that the protection register of CFM allow to secure blocks of 16Kbytes.

 

Thanks

ラベル(1)
0 件の賞賛
返信
1 解決策
1,404件の閲覧回数
mjbcswitzerland
Specialist V

Hi

 

Yes, the FLASH granularity is 4k on the M5225x family. This is twice the size as in the M5223X types.

 

Regards

 

Mark

 

www.uTasker.com
- OS, TCP/IP stack, USB, device drivers and simulator for M521X, M521XX, M5221X, M5222X, M5223X, M5225X. One package does them all - "Embedding it better..."

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,405件の閲覧回数
mjbcswitzerland
Specialist V

Hi

 

Yes, the FLASH granularity is 4k on the M5225x family. This is twice the size as in the M5223X types.

 

Regards

 

Mark

 

www.uTasker.com
- OS, TCP/IP stack, USB, device drivers and simulator for M521X, M521XX, M5221X, M5222X, M5223X, M5225X. One package does them all - "Embedding it better..."

0 件の賞賛
返信