MCF5223x PWOR function ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCF5223x PWOR function ?

2,148 次查看
MrBean
Contributor I

The PWOR bits set pins to "wired-OR".

There is no further explanation in the RM.

 

Does anyone know what it does ?

Does it disable the low side driver transistor of the pin ?

标签 (1)
0 项奖励
回复
2 回复数

1,419 次查看
mjbcswitzerland
Specialist V

Hi Mr Bean

 

I haven't used this function but I believe it is effectively setting open drain output so that several outputs can be connected together. Using a pull-up, any output driving '0' 'wins'.

 

Wired-OR is a little confusing because sometimes it is also called Wire-AND. See the following: Wired-OR

 

Regards

 

Mark

 

www.uTasker.com

0 项奖励
回复

1,418 次查看
admin
Specialist II
Yes, I think it is what is normally called open-drain output. I haven't tried it though.
0 项奖励
回复