MCF5223x PWOR function ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF5223x PWOR function ?

2,147件の閲覧回数
MrBean
Contributor I

The PWOR bits set pins to "wired-OR".

There is no further explanation in the RM.

 

Does anyone know what it does ?

Does it disable the low side driver transistor of the pin ?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,418件の閲覧回数
mjbcswitzerland
Specialist V

Hi Mr Bean

 

I haven't used this function but I believe it is effectively setting open drain output so that several outputs can be connected together. Using a pull-up, any output driving '0' 'wins'.

 

Wired-OR is a little confusing because sometimes it is also called Wire-AND. See the following: Wired-OR

 

Regards

 

Mark

 

www.uTasker.com

0 件の賞賛
返信

1,417件の閲覧回数
admin
Specialist II
Yes, I think it is what is normally called open-drain output. I haven't tried it though.
0 件の賞賛
返信