MCF52235, MCF52234:CAU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF52235, MCF52234:CAU

3,114件の閲覧回数
BIS
Contributor I
Do you know how to determine whether CAU unit is present in MCF52235 family device: in softwareI have to make choice between MCF52234( doesn't have CAU unit, sha1 algorithm is performed in software) and MCF52235 ( CAU is present, sha1 is calculated by meens of hardware unit )? Thank you for help.
ラベル(1)
0 件の賞賛
返信
4 返答(返信)

1,881件の閲覧回数
admin
Specialist II
In my opinion, Chip Identification Register is perfect for this job. See manual.
0 件の賞賛
返信

1,881件の閲覧回数
BIS
Contributor I
Thank you for help. I tried to read out processor hardware configuration loaded after reset into D0 and D1 register, but it has the same value.
0 件の賞賛
返信

1,881件の閲覧回数
admin
Specialist II
The regisiter I was referring to is part of Chip Configuration Module (CCM) and its address is IPSBAR+0x11000A. Again, see manual.
0 件の賞賛
返信

1,881件の閲覧回数
BIS
Contributor I
Yes, it works. Thank you for help. I tried to say that hw configuration information from D0,D1 after reset is the same for 52234 and 52235. And the manual approves that. The CAU present bit is always zero.
0 件の賞賛
返信