MCF52235, MCF52234:CAU

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCF52235, MCF52234:CAU

1,845 次查看
BIS
Contributor I
Do you know how to determine whether CAU unit is present in MCF52235 family device: in softwareI have to make choice between MCF52234( doesn't have CAU unit, sha1 algorithm is performed in software) and MCF52235 ( CAU is present, sha1 is calculated by meens of hardware unit )? Thank you for help.
标签 (1)
0 项奖励
回复
4 回复数

612 次查看
admin
Specialist II
In my opinion, Chip Identification Register is perfect for this job. See manual.
0 项奖励
回复

612 次查看
BIS
Contributor I
Thank you for help. I tried to read out processor hardware configuration loaded after reset into D0 and D1 register, but it has the same value.
0 项奖励
回复

612 次查看
admin
Specialist II
The regisiter I was referring to is part of Chip Configuration Module (CCM) and its address is IPSBAR+0x11000A. Again, see manual.
0 项奖励
回复

612 次查看
BIS
Contributor I
Yes, it works. Thank you for help. I tried to say that hw configuration information from D0,D1 after reset is the same for 52234 and 52235. And the manual approves that. The CAU present bit is always zero.
0 项奖励
回复