MCF52221 : UART, external interrupt : no detection of external interrupt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF52221 : UART, external interrupt : no detection of external interrupt

1,722件の閲覧回数
polo
Contributor I
Hi,
I try to use the uart 1 and the the edge port module IRQ1 in input interrupt.
My 2 codes are good separately.
But when I use both then the detection of the IRQ1 functions one time.
The UART functions at 115200bauds and IPL = 2 and all ICR are different, I use asm_set_ipl before before modify all IMR.

Someone can help me?
thanks,
Best regards

Yohan
ラベル(1)
0 件の賞賛
返信
1 返信

786件の閲覧回数
mccPaul
Contributor I
Hi
 
You need to post the code that you are using to set up and then reset each interrupt.
 
You must have something wrong.
 
Paul.
0 件の賞賛
返信