MCF52221 : UART, external interrupt : no detection of external interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCF52221 : UART, external interrupt : no detection of external interrupt

1,720 Views
polo
Contributor I
Hi,
I try to use the uart 1 and the the edge port module IRQ1 in input interrupt.
My 2 codes are good separately.
But when I use both then the detection of the IRQ1 functions one time.
The UART functions at 115200bauds and IPL = 2 and all ICR are different, I use asm_set_ipl before before modify all IMR.

Someone can help me?
thanks,
Best regards

Yohan
Labels (1)
0 Kudos
Reply
1 Reply

784 Views
mccPaul
Contributor I
Hi
 
You need to post the code that you are using to set up and then reset each interrupt.
 
You must have something wrong.
 
Paul.
0 Kudos
Reply