MCF51JM128 USB host mass-storage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF51JM128 USB host mass-storage

2,192件の閲覧回数
wo_mig
Contributor I

I am preparing to choose  MCF51JM128 as the MCU of a device which includes an USB host port using to download data to USB Flash Device or other USB storage devices.

And I want know does MCF51JM128 have enough RAM and on-chip FLASH to finish the function?

What ohter developping should I do when I use the CMX USB stack?

Is there any successful  application to access USB Flash Device?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,576件の閲覧回数
bluehacker
Contributor III

JM128 is suitable for your application. CMX USB stack is ok , JM128's flash and sram is enough for your application

 

 

0 件の賞賛
返信

1,576件の閲覧回数
DMV
Contributor I
0 件の賞賛
返信