MCF51JM128 USB host mass-storage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCF51JM128 USB host mass-storage

2,188 Views
wo_mig
Contributor I

I am preparing to choose  MCF51JM128 as the MCU of a device which includes an USB host port using to download data to USB Flash Device or other USB storage devices.

And I want know does MCF51JM128 have enough RAM and on-chip FLASH to finish the function?

What ohter developping should I do when I use the CMX USB stack?

Is there any successful  application to access USB Flash Device?

Labels (1)
0 Kudos
Reply
2 Replies

1,572 Views
bluehacker
Contributor III

JM128 is suitable for your application. CMX USB stack is ok , JM128's flash and sram is enough for your application

 

 

0 Kudos
Reply

1,572 Views
DMV
Contributor I
0 Kudos
Reply