MCF51JM128 Bootloader AN3748

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCF51JM128 Bootloader AN3748

3,440 Views
lucas_loizaga
Contributor I

Hi!

Over 5 years ago FSL support sent me the source code of the application of PC AN3748.
Currently I need to run this AN using Windows 64 bits.
The package was updated with AN3748 compatible drivers, but these drivers do not work with the original PC application.
Please could someone from NXP or FSL post the updated source code of the PC application?

Thank you very much,

 

Lucas

Labels (1)
0 Kudos
Reply
3 Replies

3,188 Views
dariobalina
Contributor I

Hi,

Anyone have backuped the zip containig the AN3748 source code?

There are no traces of it on the web, It seems that many of Freescale's old application notes resources have been removed.

Thank you very much,

Dario

0 Kudos
Reply

3,188 Views
lucas_loizaga
Contributor I

Hello!, anybody here?

0 Kudos
Reply

3,186 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Lucas 

Please check the attached file, this is the last version that I have, 

I hope this will help you.

Regards

Vicente Gomez

0 Kudos
Reply